各位好,想请教下,TPS54310的软启动控制电容Css是接在哪两端的?有参考电路图吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,一般芯片SS的电容都是接在SS引脚和地之间的。下面是用TPS54310做一个同步降压电路的参考设计文档,另外楼主也可以使用webench来进行自己的设计。
不好意思,上传附件错了,下面这个应该可以直接下载。
非常感谢,你们蛮辛苦的哈,这么早就回复我的帖子!另外,这块芯片的热阻大吗?我用这款芯片实现5V转3.3V,输出电流在1.2A左右!
好的,如果我不用soft-start功能,是不是将SS/ENA通过电阻下拉到地,谢谢!
期待您的回复!
楼主,这个引脚可以用作使能端,做输入欠压保护,直接两个分压电阻分压到设定电压就可以了。楼主直接上拉可以再稍微大些,10K可以。
楼主,很高兴你能找到答案,问题如果解决了,请把问题close掉。谢谢使用TI的产品。