如题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
LM3444 是恒定关断时间的AC/DC恒流控制器。关断时间的长短可以通过调整与Coff pin连接的电容大小来控制。正常工作时,当与LED串联的开关管关断时,电流会通过PNP给Coff pin上连接的电容充电。当Coff的电压高于内部比较器的1.276V时,IC输出的PWM控制信号会开通开关管,同时Coff pin内部的下拉管开通,使Coff pin上连接的电容放电,系统进入一个新的周期。因此,Coff上的电容越大,充电时间就越长,关断时间也就越长。
你可以参考data sheet 12页和13页上的公式来计算关断时间和相应的开关频率。
谢谢!