TI技术支持你好:我用tps2540做充电器,现在遇到一个问题:在输入电源功率足够的情况下,连接iPad充电时,充电电流只有800-900mA;
查找资料得知iPad的充电规范是5.1V,D+是2.7V电压,D-是2.0V电压;
从tps2540的规格书中可以看到Driver mode下可以提供D+是2.0V电压,D-是2.7V电压,正好相反;
我做过如下测试,在充电的usb端口将usb信号引出来,将D+和D-交换,再测试,充电电流可达到1400mA,但是还是达不到iPad的标称充电电流2.1A;
总结,问题1:tps2540是否有一种模式支持iPad2.1A的标称充电??
问题2:为什么将充电端口的D+,D-交换符合iPad的充电规范后还是不能达到标称充电电流2.1A?是不是tps2540无法输出2.1A电流;