This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: 电源VIN1或VIN2输入功率从过小到恢复到标准功率时,需要断开并重新接VIN1/2时,才能恢复充电,为什么?

Part Number: BQ25798


利用BQ25798EVM板来测试充放电时,发现VIN1或VIN2功率下降到一定的程度后,VIN1或VIN2重新恢复功率后,BQ25798不能自己恢复充电,而是必须先将VIN12电源断开,然后再重新接上去,才能恢复充电。请问这上什么原因导致的?需要设置那些参数?BQ25798EVM的参数都是默认的,没有修改。

例如:

VIN1或VIN2在12V-500mA电源下,可以正常充电。当电流降到10mA(利用恒流源来限制输出电流)后,BQ25798不给电池充电。然后再将恢复到500mA以上,BQ25798不会给电池充电。必须将VIN1或VIN2断开并重新上电,BQ25798才能正常充电。