This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

模拟量隔离直流电路



一、主要目标

       工业现场的干扰信号复杂多样,为了提高产品工作的可靠性和安全性,需要开发一种模拟量隔离电路,串接在DCS控制系统的信号输出端与被控设备的输入信号端之间,隔离外部各种干扰信号。

二、基本条件

1、模拟量输入:0~10V电压。

2、模拟量输出:0~10V电压。

3、供电电源:DC  24V

4、采用常规元器件完成隔离电路的开发,低成本。

三、主要技术指标

1、输入阻抗:>100 kΩ

2、输出阻抗:<1 kΩ

3、输出精度: <1%

4、传输带宽:100 kHz

5、隔离性:输入、输出、电源侧之间隔离电压1000 Vac