This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电池管理芯片MAX17005B系列推荐电路中的一个问题

Other Parts Discussed in Thread: BQ24735, BQ24725

最近,公司准备选用MAX17006B做电池充放电管理,在其Datasheet第10页的推荐电路中,有个N4的NMOS的作用是什么,资料中描述说是:When the adapter voltage is removed, the charger stops generating BST refresh pulses and N4 forces N2 off,这个描述有点简单,具体N4怎样导致N2 off?可否将N4去掉?

  • 你好,

    或许是其Datasheet写错了,我认为N2应该为N3,当输入adapter拔掉后,N4导通,使得N3断开。

    不知您的应用是什么,推荐您使用TI的BQ24725和BQ24735,都是3.5*3.5mmQFN封装;支持1-4节锂电池;不需要任何补偿电路;集成有独立的ACFET驱动和BATFET驱动,能更方便的实现路径管理功能。同时BQ24735还有turbo boost功能,其DCDC converter可以工作在boost模式,由adapter和电池一起为系统供电。

  • 你好,

    是的,有可能是datasheet写错了,弄得我没法理解。我今天仔细看看你推荐的TI  BQ24725和BQ24735,看能否满足我们的要求。如果OK,选择其中一款。如有什么问题,再咨询你们,非常谢谢!

  • 你好,我们可以提供BQ24725  这颗料价格非常有优势,有需求可以联系我。

    ichk1688@gmail.com