This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS71710 over output



my design is

:input 3.3V,

:EN connect to VIN through 10kohm resistor,

:input and out capacitor is 1uF,NR capacitor is 10nF

with no load output is 2.2V

Has this been damaged? or other reasons?

POWER.pdf