This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于bq3060的问题

Other Parts Discussed in Thread: BQ3060

1.我在gas gauging state中设置容量为5000mAh,为什么在sbs显示的full charge capacity为4912呢?这个是什么问题?


2.现在在充电过程中,目前电量显示为66%,电池电压分别为3.389v和3.421v,这是CHARGING STATUS中的FAMTO和OCHGI分别为1.我看说明书是charging fault,我现在设置的充电电流为0.5A,在charge control里我是用的都是默认值。


3.目前充电到了100%,但是下一次重新使用,然后刷新电池电量就变为18%,又得继续充电,这是怎么回事?、


4. 充电中我设置的电池的过压是3700mv,现在一个电池电压超过了,怎么没有反应,也不关断,还在充电,这个设置有什么不对?


5,上次我设置好了放电,有节电池电流基本放为了零,严重不平衡,我设置不平衡也是默认值。这个是什么情况,怎么没有关断呢?