This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

负载开关TPS22968工作在防反向电流模式下的最大导通电流还是4A吗?

Other Parts Discussed in Thread: TPS22968

TPS22968是个双通道的负载开关,其数据手册中P20-Figure 36又讲到将VOUT1与VOUT2相连,使用VIN2作为开关的输出端,这种连接方式可以起到防止电流倒灌到输入端。

但是,使用这样的连接方式,负载开关本身的最大导通电流还是4A吗?因为各种连接方式,实际是将两个源级连接在一起。当开关导通时,电流是不是先通过第一个N-MOS流过,然后再通过第二个N -MOS的寄生二极管流出的?如果是,寄生二极管的最大电流也是4A吗?

就是些模电的基本问题,求科普。