This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【原创】+手机电池充电器设计

Other Parts Discussed in Thread: BQ24086, BQ24085

首先让我们了解下,我们这次设计的IC:BQ24086

以下是官方的介绍:

The bq24085/6/7/8 series are highly integrated Li-Ion and Li-Pol linear chargers, targeted at space-limited portable applications. The bq24085/6/7/8 series offers a variety of safety features and functional options, while still implementing a complete charging system in a small package. The battery is charged in three phases: conditioning, constant or thermally regulated current, and constant voltage. Charge is terminated based on minimum current. An internal programmable charge timer provides a backup safety feature for charge termination and is dynamically adjusted during the thermal regulation phase. The bq24085/6/7/8 automatically restarts the charge if the battery voltage falls below an internal threshold; sleep mode is set when the external input supply is removed. Multiple versions of this device family enable easy design of the bq24085/6/7/8 in cradle chargers or in the end equipment, while using low cost or high-end AC adapters. 

设计时唯一比较奇怪的是,使用WEBENCH时好像没找到这个BQ24086IC,所以使用的是官方的原理图。

BQ24086(具有热调节的 750mA 单片锂离子/锂聚合物充电管理 IC)芯片。