在使用LM5069-2测试功率限制功能的时候,发现电路并没有按照设定的电流进行限制,Vin=24v,Rsns=20mR,Rpwr=50k,Ctimer=470nf,在使用负载仪测试的时候,电流限制功能能正常工作,I=2.75A左右,电路会正常断开,测试功率限制时,并不会将电路断开,按照9.2.1.2.3计算,50k电阻设定Plim为20W左右,所以很疑惑,Rsns是否设定的是瞬时状态的电流值,保证surge不会太高,而Rpwr设定的是正常工作时候的电流值,所以,Plim需要如何进行测试是否正常工作,通过负载仪只能测出来Rsns设定的电流值是OK的,Rpwr还不是很明白怎么影响输出功率限制的,希望得到帮助,谢谢