This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25088使用纹波太大

Other Parts Discussed in Thread: LM25118

您好,做一个5v、5A的电源,输入直流18.8v,电路参考TI评估板电路

电路PCB布局也参考了TI设计,输出4.96v基本正常,但是纹波太大,有600mv,电路有些参数没有严格按照TI的设计,因为元件有限,其中电感值为8.2uH,请问这问这是什么问题引起的纹波这么大?纹波频率在200kHz左右。

  • 可以增大电感,同时采用低ESR的电解电容。

  • 你好,根据你的描述,建议你从如下几点着手分析:

    (1)空载时输出电压波形是怎样的,稳定吗?

    (2)如果空载即输出不稳定,即有可能是环路不稳定的原因导致,可优化外围补偿器件参数;可在反馈分压电阻(R7)上并联1pcs小电容,看看有无改善;

    (3)如果帯载之后纹波很大,查看开关结点波形,有无大小波,如果开关结点波形正常,应该还是环路的问题。

    综上,建议贴上测试波形,便于大家分析。

  • Hi

       将输出的一个47uF换到输入(另一个去掉),而将输入的2个2.2uF的陶瓷电容改到输出。

        这样可以增加输入得稳定性,和减小输出电容的ESR, 看是否有改善(最好还确认一下补偿参数)

  • 请参考LM25118 user guide输出电容设置,电感之后先是47uF陶瓷电容,再是电解电容,最后是高频滤波电容