This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z45-R1如何永久性的退出ship模式

Other Parts Discussed in Thread: BQ20Z45, BQ24617, BQ78350

各位好,我现在正在使用BQ20Z45-R1想问一下如何永久性的退出ship模式,我买的新芯片上点接上电池包后(两节串联7.2V),要把CELL+和PACK+短接才能实现芯片与EV2300的通信,查看了论坛是进入了ship模式,那如何永久的退出这个模式呢?现在是跳着飞线的,以及在以后产品量产的时候,如何处理这个要把CELL+和PACK+短接才能实现芯片与EV2300的通信的麻烦步骤

  • 您好,

    芯片出厂是会处在shutdown的模式下,你也可以通过在pack+和pack-端外加电压来激活芯片,如接入充电器就可以将IC激活。

  • 几种情况会进入ship模式

    1.上电POR

    2.欠压

    3.接收到进入ship mode的命令

    所以如果不想进入ship 模式的话,那么点接后比较有可能出现ship mode情形的是欠压, 此时是需要连接适配器去充电,自然就满足激活条件。

  • 1.现在我的情况是点接后,ev2300可以和芯片正常通信,但如果把电池包移除,再接入电池包,芯片就需要再次点接,这个情况如何避免?类似于客户要更换电池包,就要把原有的电池包卸下来,装上新的电池包。这个时候就需要重新激活。

    2.另外我搭配的充电芯片是bq24617.现在的现象是,如果不打开BQ20z45上的dsg和chg MOS管,bq24617能输出8.4V的充电电压,如果把dsg和chg打开,bq24617就不工作,两个充电电路上的mos就没有开关动作,充电指示灯也不亮,不知道是什么原因,是否有调试的意见??

  • 蔡工,我的bq78350接到上位机后,只要写数据就会出现找不到设备的情况,这是为什么?