输入:16V-40VDC;输出:5V/1.5A、±15V/0.25A;输入与输出隔离。
有没有内置开关及控制器的芯片型号,尺寸要越小越好,做2个反激电源。最好单芯片,2个PWM独立控制的芯片。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以用sample swither这类芯片做,例如LM2587,L2588.
可以用一个芯片来做,当然也可以分开用2个芯片来做。
用谐振复位的方案,三路从一个变压器出来,这样效率最高,电路简单,稳压要求高的可以在次级增加线性稳压电路
选一个8脚芯片, 带基本保护就行, 变压器里绕组设置好两路输出.用基本的稳压管限定. 比如LM系列