This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS76901-HT: 参考电压不对

Part Number: TPS76901-HT


你好!请教一下,我使用的是TPS76901SHKJ这种耐高温电源芯片,我从手册上得知该芯片的输出电压通过公式得到,输出电压的得到与参考电压以及接入的R1与R2有关,与输入无关。我于是采用5V的输入供电,R1与R2分别接入94千欧与170千欧,该芯片手册上的参考电压为1.16V,我通过公式计算理论得到应该是1.8V。

但是我通过实际测试得到的电压是2.2V,FB参考电压的引脚是1.47V。于是我开始查找原因,我发现焊接并没有问题,我从论坛帖子上看到,是否是因为空载的原因,于是我将输出接了一个10千欧的负载,FB这个引脚变为了1.02V,输出变成了1.6V。

我尝试将芯片输入电压5V改变为5.5V时,我发现这个FB引脚与输出电压变成1.07V与1.68V

我尝试将芯片输入电压5.5V改变为6V时,我发现这个FB引脚与输出电压变成1.12V与1.77V

从测试结果来看这个输入电压直接影响到输出与参考电压

而手册上表示这个参考电压应该是固定的1.16V,究竟是什么问题,请帮我分析一下!

电路我是借鉴了这个