請問一下我是使用湯淺REC14-12,我要去哪裡取得對應的Chemistry ID?或是我變更電池要如何快速取得Chemistry ID?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CHEM-ID选择
A电池先采用0.5C恒流,恒压taper电流小于0.01C充饱
B静置2小时
C连接EVM板,自动log DataRAM数据,间隔为4s一次
D开始用0.1C电流放电,一直放到2.8V(或者电池最低放电电压)
E静置5小时
F将以上的log的数据保存下来用MATHCAD程序计算CHEM_ID,软件链接http://www.ti.com/litv/zip/sluc138bh
G 通过bqCONFIG/EVSW/Gauge studio相应界面下载CHEM_ID
注意板在做CHEM_ID前要先校准好,放电过程要连续,记录的数据包含放电完之后静置的那5小时,
請問我有BQ34Z100的EVM,但是我實際要用的是BQ34Z110,請問我可以用BQ34Z100的EVM去測鉛蓄電池的數據嗎?要放到幾伏特?
MATHCAD程序计算CHEM_ID,软件链接http://www.ti.com/litv/zip/sluc138bh 這個連結沒東西?MATCHCAD是一套應用程式?