This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好:
我正在使用DMX512协议做调光控制,目前有几个接口传输方面的问题。
下图是TI 工程师Brett Larimore写的一份Application Report(SPRABR9–January 2013)中的截图:
我的问题是:上图中RS485接口转换芯片SN65HVD3082ED的传输速率只有200Kbps, DMX512标准为250Kbps,这样做可行吗?
另外,SN65HVD3082ED的供电为5V,转换后的串行信号(DMX-RX)能直接接到3.3V供电的TMSF28027 MCU的SCI引脚上去,这样电平兼容吗?
Hi, Helena
那请问在这份文档(见附件)里面TI的设计是直接接到Piccolo MCU的SDI引脚上去了呢?