This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260不能正确输出设计电压的问题

Other Parts Discussed in Thread: TPS54260

我现在在用TPS54260做一款GPS/GSM产品,结果发现输出的电压和设计的不一样!找不到问题出在哪里?请大家帮忙看看?
 

  • 你好,初步看了一下,觉得可从如下方面排查原因:

    (1)芯片是否使能工作了?

    (2)1脚与10脚之间的boot电容容值是否过小?一般都是选取0.01uF或更大,规格书中使用的是0.1uF的典型值;

    (3)空载输出电压是否正常?空载电压不正常的话,那就看看你电路是否有虚焊或者错焊的情况;

    (4)帯载是否正常?注意IC内部集成MOS,有内部过流保护点。

  • (1)设定电压与实际电压有多大区别

    (2)电路板是否完整

    (3)输入  enable 是否正常

    (4)boost sw 是否正常

  • C8电容太小了,应该为0.1uF

    请测量C20的电压

  • Hi 

         除了chargepump的电容太小导致的驱动力不足之外,layout上可能存在问题。D4应该选择是的超快回复的肖特基二极管,而不是TVS管,D4的作用是续流,不是稳压。

  • Hi 

        建议您先采用肖特基二极管,然后测试输出是否稳压?

        其次在芯片的Vin脚上焊接2个10uF的电容(或者是尽量靠近Vin脚),再测试,确认输出是否稳定在3.8V?(可以带一定的负载,之所以这样是因为从您的电路上看,可能是输入电容layout比较远导致瞬态转换是输入电压大幅跌落导致的,也就是输入没有稳压)

  • 兄弟,C8太小了,储存的能量根本不足以驱动内部MOS管,电路怎么可能正常工作啊。