This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z45R1的PF status中RSVD被置1,芯片不能正常工作



今天调BQ20Z45R1的时候出现了如题的报警,PF status中RSVD被置1。过程是这样的。我先没接电池包,而是在pack+。pack-之间加了8.4V的充电电压,EV2300可以连接,并读取状态寄存器。但是出现了如题的报警,放电mos和充电mos都被关闭。但是RSVD不是预留的bit吗,按理说不会被置1.这个时候,接入电池包,也不能正常工作,如果拔掉充电器,那么连芯片的寄存器都不能正常读取。只能重新烧senc后,再重新导入gg文件,芯片才能正常工作。我想问一下,为什么在不加电池包的情况下,在pack+。pack-之间加电压会让芯片出现这个现象,就是预留位被置1.具体就是图片中的那个红圈的FLAG