各位老师好!
计划设计一新产品,初选INA333作运放,ADS1255IDB作AD,还有测量传感器需供电,最好是用9V供电,这些电路的供电要求都比较高,还有AD的基准电压,请教老师们建议一下使用哪些高精度的稳压芯片比较好;有没有9V以上电压的基准芯片,便于做9V电源。或者有没有9V高精度稳压芯片。
谢谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
供电电压对精度的要求不高的话可以选择TPS7A4901这类高性能的LDO: http://www.ti.com.cn/product/cn/tps7a4901
应该是LP38798
Input Voltage Range: 3 to 20V
Output Voltage Range :1.2 to 19.65V
Ultra-Low Output Noise: 5 µVRMS (10Hz to 100KHz)
High PSRR: 90 dB at 10 kHz, 60 dB at 100 kHz