This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5009: 9通道LED Driver

Part Number: LP5009


Hi,

请帮忙推荐合适物料,谢谢!

需求如下:

  • 器件类型:LED驱动IC
  • 通道数9(满足实际使用7个通道数就可以);
  • 封装大小:≤3*3mm
  • 驱动电流:7LED灯,每颗灯的驱动电流是1~3mA
  • 工作电压:2.4-5.5V
  • 芯片工作电流:<30uA
  • 控制引脚:I2CEN,接口可兼容1.8V通信。(主芯片是1.8V供电)