This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601: 充电电流不能配置

Part Number: BQ25601


由于充电器输出电流限制(约1.5A),想把充电电流由默认的2A改为1A,但修改了寄存器REG02(由默认的A2改为91),充电过程中读取该寄存器,其值自动在A2和91(一会A2,一会91)之间变化,充电电流也随之在1.5A和1A间变化。这是什么原因?

  • 您好,To keep the device in host mode, the host has to reset the watchdog timer by writing 1 to WD_RST bit before the watchdog timer expires (WATCHDOG_FAULT bit is set), or disable watchdog timer by setting WATCHDOG bits REG05[5:4] = 00.