在开发的过程中,遇到这样的问题还望解答,当我设置过流保护值为20A时,15A就保护,当设置为40A时30A左右就保护了,基本上是正确的保护值乘以个0.75它就保护,采样电阻为2.5毫欧,用万用表测的采样值是正确的,还有没有其他的因素导致这个偏移。应该怎么解决。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在开发的过程中,遇到这样的问题还望解答,当我设置过流保护值为20A时,15A就保护,当设置为40A时30A左右就保护了,基本上是正确的保护值乘以个0.75它就保护,采样电阻为2.5毫欧,用万用表测的采样值是正确的,还有没有其他的因素导致这个偏移。应该怎么解决。
分别是50.2mv和100.1mv,采样部分是正确的。并且根据16 bit adc cc_hi 和cc_lo2个寄存器计算出的电流值是正确的,就是在保护的时候有这个偏差。
我想问一下 08寄存器的保留位不为0的话会有什么影响? 什么情况下 导致保留位不为0?
我的影响是在过流保护的时候会出现偏差,给0x8寄存器的保留位赋值为1的时候可能会改变保留位的值。
请问到底是该为零还是不该为零。
手册上看到0x08低四位为保留位,应为1000,初始化的时候需要写1000吗
你好,我想问一下你的BQ76930是用单片机控制的,还是TI的开发板啊。我在测电流过程中误差很大啊,不知道是什么原因,现在急用,找不到原因,望大侠赐教啊,非常感谢!
BQ76930做短路保护,用差分探头测电流检测引脚怎么开始有负压?如果是电感造成也应该是正向的
附件为:1通道为MOS驱动波形
2通道为MOS管耐压
3通道为电流检测波形
4通道为短路电流波形
很明显电流检测波形有个负压,导致MOS大电流开通200us