This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504: Does this chip have multiple versions

Part Number: BQ25504


Hello!

When browsing the data manual of BQ25504, I noticed that its cold start voltage was changed from 330 mV to 600 mV in 2015, as well as some other parameter changes. Do these changes mean that there are multiple versions of BQ25504. I am afraid that there will be differences in the performance of BQ25504 purchased during different production periods.

Thank you!

WZG