看附件电路,如何去使用pwm去控制提供给lcd的背光(VLED+,VLED-)???????????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看附件电路,如何去使用pwm去控制提供给lcd的背光(VLED+,VLED-)???????????
请参见TI专家的回复:
能否提供AT070TN92的部分说明书,因为我只对LCD供电部分熟悉,AT070TN92面板电压: 3.3/10.4/16.0/-7.0V (Typ.)(VCC/AVDD/VGH/VGL)这些都有了 , 在AT070TN92的CN上只是提供了VLED+这个脚,那么在LCD控制屏内部是否有电路来控制LED的背光亮度?
通常对LED PWM调光,可以通过MOS控制VLED 9.3V的电压,当MOS开,供电9.3V即满亮度,当MOS关,即零亮度,而MOS开关的PWM 占空比即可调节背光亮度,因为人眼分辨不出开和关的控制,所表现出来的就是亮度变化。