This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于低温电量很不准确的问题:BQ27541



你好!单节4000mAh的电池,采用BQ27541,常温时,容量误差在3%左右;但放入低温箱,-20的环境下放电,放了接近400mAh容量时,才从100%变成90%,到电量显示为29%时,放不出电来,从曲线来看,误差大约为:30%。请问:是哪个环节出问题了?是否有温度补偿设置。谢谢!

  •  

    这个现象是由于常温充电的话会比低温充进更多的能量,所以常温充饱对于低温相当于是过充,电量计会在100%停滞一段时间放出过充容量。 另外对于-20C低温测试,首先需要确保CHEM-ID是专门制作的而不是通过MATCHCAD匹配得到的,其次再根据测试结果调整 T Rise T time constant,以及Resrelax这几个参数。

    另外这个是什么应用会测试到-20C的温度,普通电池此时的容量会非常少。

  • 我们的产品也是要求-40℃正常工作。现在的情况是在-40℃时,有一块电池的电量读出来的0%,一块电池的电量是100%,这两块电池在常温下的电池电量分别是99%和100%。请教一下需要怎么专门制作一个CHEM-ID,以及怎么调整T Rise T timie constant 以及Resrelax这几个参数呢?在线等,急用。跪谢。

  • 请问下,你们的BQ27541低温电量不准的问题是怎么解决的呢?谢谢!