This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急!!!升压直流电源类问题,在线等大神指导~~~~~~~



我们想设计并制作一个输入为10V~14V直流电压,输出为24V的高效率升压直流电源。
它的基本要求是:在50欧姆负载上,
(1)在输入电压为12V时,其输出电压为24V直流;
(2)在输出电压为24V时,尽可能减小输出电压纹波;
(3)升压直流电源效率应大于75%,并尽可能提高效率;
(4)在规定的负载电流范围内,尽量减小负载电流调整率;
(5)输入电压在10V~14V之间变化时,尽量降低电压调整率。

但我们现在设计出来的电路图有一点问题,我们不知道问题出在哪里,希望有好心人能帮忙解决一下,感激不尽!!

附件使我们用TINA做的仿真。

1.TSC