This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24296 充电电流的设置



你好,我们的电路把Psel与OTG接高电平,ILIM我接360R的电阻,这时用IIC接口来控制电池的充电电流,可以吗?我想把电流设在500MA,1500MA可以吗?

  • 你好,

    PSEL和OTG是决定上电后input current limit寄存器的值,若PSEL和OTG都为高,则Vbus上电后REG00[0:2]被设置为010,对应500mA。之后可以通过I2C来设置这个寄存器为不同的输入限流值。

    但实际的input current limit是由寄存器REG00[0:2]所设置的值和由RILIM电阻所设置的值中较小的那个决定。如你用360R电阻,RILIM设置的input current limit约为1.2A,当寄存器设置的值小于1.2A时(可以为100mA,500mA,900mA,1A),实际input current limit就为寄存器设置的值。若寄存器设置的大于1.2A(可以为1.5A, 2A, 3A),实际input current limit 就为1.2A。