1、在E-BIKE应用,是否可以将CHGST管脚串联电阻后直接焊接至PACK+?
2、在BQ77910 DEMO测试中,我们将R50&R52换成50m欧电阻,充电电流控制在200mA以下,接充电器时,总是提示充电短路(Short Circuit Chg),请帮忙解释?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、在E-BIKE应用,是否可以将CHGST管脚串联电阻后直接焊接至PACK+?
2、在BQ77910 DEMO测试中,我们将R50&R52换成50m欧电阻,充电电流控制在200mA以下,接充电器时,总是提示充电短路(Short Circuit Chg),请帮忙解释?
谢谢!
CHGST :Charger-status input, used to detect charger connection/wakeup,不建议直接串联电阻直接接到PACK+; TI已经给出最新这部分的电路,如下图:
2.R50,R52是侦测电流电阻,Short Circuit Chg的可写电压范围是-10mV~-425mV. 如果你用的50mO的电阻太大了,当然200mA是的电阻上电压早超过保护电压范围,就保护了,所以,此侦测电流电阻,不要选择这么大,用参考电路中2MO的就可以了。
chris,谢谢你的回复,我们尝试一下你推荐的电路。
还有一点疑问是,我们采用的Short Circuit Chg电压是-10mV,对应50mO电阻,报警电流是200mA,那么我们使用200mA以下充电电流的充电器时,不应该提示Short Circuit Chg,但是实际CHGST连接在PACK+,每次接入充电器,都会提示Short Circuit Chg,导致不能充电,请帮忙解答,谢谢!
Hi Peter
910本身技术文件上已经说明,相匹配的Current-Sense Resistor是1mO的,所以你使用50mO的可能会出现一些问题,所以还是建议你把R50,R52换成2mO的,此问题应该就不会存在。