This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3489 DC-DC controller 外部PMOS使用PMPB27EP可以实现Iout到4A吗?

Other Parts Discussed in Thread: LM3489

从选型列表中看到LM3489比较符合设计规格,打算使用...

但是看datasheet中typical电路 Iout最大值都在1A以下,有点担心...如果我使用的外部Power Stage component符合datasheet中设计值,Iout可以到4A吧?PMOS打算使用PMPB27EP,型号如附件,是否会有什么风险?

另外设计比较关注output ripple voltage,datasheet中提到VOUT_PP= VHYST(R1 + R2) / R2,这样看起来如果Vin=25V,Vout=5V这种应用VOUT_PP会很大...

后面提到使用Cff加速电容可以减小VOUT_PP...可以减小到多少呢?有公式大概可以计算出吗?

感谢!

PMPB27EP.pdf