This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: VC1和VC0短路

Part Number: BQ76930


你好,

我们使用两颗BQ76930芯片,通过级联的方式作出20S1P(18650)的电池管理方案;在电池组批量生产过程中,出现了一部分主板损坏的现象。

通过初步分析,是高侧(B11-B20)的BQ76930损坏了,B11的采样脚对B10采样脚短路,万用表测量仅约0.3Ω。

这对我们的生产造成了困扰,我有两个问题希望可以得到解答,

1.电压采样线的焊接顺序对芯片有没有影响;

2.什么原因会造成两个采样脚短路的现象呢?

诚盼回复,谢谢