This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3818 CCM APFC 在230V时,重在PF值是多少?

Other Parts Discussed in Thread: UCC3818, UCC28070

您好!

       我用UCC3818做BOOSTPFC时,   在AC  230V时,  PF值只有》0.93,  请问还有上升空间吗?

还有请问, CCM模式的PFC一般的效率是多少(从AC输入到385V)?

现在TI有  ZVS  PFC的芯片吗?

  • 1.有上升的空间,一般通信电源的PFC在半载以上PF指标都要求大于0.99,所以您的电路是有优化的空间,而且该指标对你电路的效率也是有影响,建议关注一下采样和补偿环节。

    2.对于传统的CCM的BOOST电路PFC,电路设计合理的话峰值效率能到96%以上,采用无桥或者交错式BCM等技术的话峰值效率甚至能到98%,你可以关注一下UCC28070(www.ti.com/.../ucc28070)。

    3.根据个人了解的情况,TI可能没有ZVS的芯片,详细信息,你可以查阅TI的2011年最新中文电源管理产品选型指南(www.deyisupport.com/.../228.aspx)。

  • 效率要看输入电压范围,用老的IC3854硬开关,在正常输入效率都在96%左右。PFC控制IC的PF值,半载以上功率因数应该要大于0.99