Other Parts Discussed in Thread: UCC3818, UCC28070
您好!
我用UCC3818做BOOSTPFC时, 在AC 230V时, PF值只有》0.93, 请问还有上升空间吗?
还有请问, CCM模式的PFC一般的效率是多少(从AC输入到385V)?
现在TI有 ZVS PFC的芯片吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.有上升的空间,一般通信电源的PFC在半载以上PF指标都要求大于0.99,所以您的电路是有优化的空间,而且该指标对你电路的效率也是有影响,建议关注一下采样和补偿环节。
2.对于传统的CCM的BOOST电路PFC,电路设计合理的话峰值效率能到96%以上,采用无桥或者交错式BCM等技术的话峰值效率甚至能到98%,你可以关注一下UCC28070(www.ti.com/.../ucc28070)。
3.根据个人了解的情况,TI可能没有ZVS的芯片,详细信息,你可以查阅TI的2011年最新中文电源管理产品选型指南(www.deyisupport.com/.../228.aspx)。