Other Parts Discussed in Thread: TPS61030, LM3489, TPS61230, TPS63020
tps61030按照官方设计的PCB,只是PowerPAD简单接GND,没有大块覆锡。通电测试一会就坏掉了,VBAT管脚对地短路。不知何故?是芯片有问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
建议先看看资料
The LM3489 is a high efficiency PFET switching regulator controller that can be used to quickly and easily develop a small, cost effective, switching buck regulator for a wide range of applications. The hysteretic control architecture provides for simple design without any control loop stability concerns using a wide variety of external components. The PFET architecture also allows for low component count as well as ultra-low dropout, 100% duty cycle operation. Another benefit is high efficiency operation at light loads without an increase in output ripple. A dedicated Enable Pin provides a shutdown mode drawing only 7µA. Leaving the Enable Pin unconnected defaults to on.Current limit protection can be implemented by measuring the voltage across the PFET’s RDS(ON), thus eliminating the need for a sense resistor. A sense resistor may be used to improve current limit accuracy if desired. The cycle-by-cycle current limit can be adjusted with a single resistor, ensuring safe operation over a range of output currents.
http://www.ti.com.cn/product/cn/lm3489
首先要确实是一上电就坏了么?如果是一上电就坏,那么可能是你电路的设计问题,
如果是工作了很长时候坏的,看一下是不是芯片太热了?
实测下芯片的温度看是否超标了,是不是温度过高把芯片搞坏了。。
很久没用它了,我烧了十几片。
EN悬空为不确定状态,不是低电平,所以会使能输出。
总结了一下烧的原因:
1. 散热大焊盘没焊接好
2. 上电很容易烧
3. 此芯片抗干扰能力不行,工作期间摸一下就烧
嗯 ,此外上电后我用示波器量了一下SW端,他的曲线不是平的而是有一个很大的峰刺。
我想做一个升压电路供电电压在3V左右 升压到4V最大负载电流能够达到2A,有那款芯片稳定性较好的,给推荐个
嗯 61030这款芯片稳定性确实不高,测试两块一块有问题 一块木问题
TPS63020 是buck boost 芯片。 主要用于最大输入电压大于输出电压,最小输入电压小于输出电压的情况。
如果输入电压总是小于输出电压,用boost变换器就可以了
谢谢
布局布板要求很高,还要到厂家做板子,机器焊接估计能达到要求
以前小米的移动电源还用它耶
大神 现在我用tps61030做的升压电路可以工作了 但负载电流达不到 负载电流1A时IC就开始发热了 这是什么原因
我做的达到2A没问题,注意你的布局布线和电感的选择,请参照tps61030—evm datasheet来布局布线
嗯 能给我简单介绍下这个芯片在布线布局上应该注意的地方吗 还有这个电感的选择 除了感值是不是还与他的饱和电流有关 我查了下我用的电感的饱和电流只有2A不知道有没有这个原因
电感尽量选择4A的功率电感,
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=slvu080&fileType=pdf
http://www.ti.com/lit/ug/sbvu006/sbvu006.pdf
这两篇pdf看看吧