This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

讨论一个多路电源方案



最近有帮朋友做一个方案,需求如下,看看大家有没有好的建议:

(1)输入交流AC(90~265Vac)

(2)输出直流,2.75Vdc or 4Vdc or 4.5V,即输出电压有三种情况,要么输出2.75V,要么4V,要么4.5V(貌似可以通过单个单刀双掷开关实现)

(3)输出路数,需要20路输出完全一致;但各路输出之间的电压可以不一样;

(4)所有输出可以直接串联,且不影响相互间的电压输出;