This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【原创】LED背光源的输出辉度计算



关于背光源辉度的计算公式 

LED光通量:L/流明
LED发光强度:I/cd
LED数量:n
反射板反射率:A
扩散板透射率: B
增光膜/偏光膜总增益:C
导光板面积:S/平方米
导光模组效率:eff

根据我的摸索,总结的公式是输出辉度=n*L*A*B*C*eff/(S*π)
比如一个7“导光板(16:9时面积为0.0135m2),LED亮度为10lm,采用15颗灯,光学设计效率是70%,反射板反射率95%,扩散板透射率92%,增光膜增益为2,
计算输出辉度为=15*10*95%*92%*2*70%/(0.0135*3.1415926)=4327cd/m2
如果再加上LCD屏,一般屏的透射率5%,则屏前输出辉度=4327*5%=216cd/m2

这里的π,是弧度计算系数,与实际值有较大差异