Other Parts Discussed in Thread: UCC3817, UCC3818
原来的电路是PFC+相移全桥的。
但是现在要求是输入变为130V—300V的宽直流输入电压。原来的PFC芯片就不合用了。要把电路中的PFC部分改为普通的BOOST。输出电压我暂时定位350V。但是当时设计的功率是3000W的。我查了一下。ti也没有相关大功率的设计方案,最好有软开关。请问有相关的芯片介绍吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PFC的输入即可以是交流也可以是直流, 130Vdc~300Vdc输入是符合90Vac~265Vac输入规格的。如果您手头有原来的产品,可以输入直流看看。