第一次是用电源芯片,在使用上有些疑惑
1.5V1A的适配器,使用默认值是否会限制输入电压和电流?
2.使用电源适配器时升压模式能否打开,难道每次需要升压都要将设置REG01[5:4]=10/11,不升压时就得改回01 ?
3.D+/D-这个怎么使用,REG08-0A数据怎么获得?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
第一次是用电源芯片,在使用上有些疑惑
1.5V1A的适配器,使用默认值是否会限制输入电压和电流?
2.使用电源适配器时升压模式能否打开,难道每次需要升压都要将设置REG01[5:4]=10/11,不升压时就得改回01 ?
3.D+/D-这个怎么使用,REG08-0A数据怎么获得?
楼主,
问题1 :如果你说的默认是BQ24195工作在默认状态,那么此时默认的输出限流是100mA。即使你用5V1A的适配器,输入仍然只拉100mA的电流。
问题2:使用稳压器时,不需要打开BOOST模式,BQ24195可以检测输入adapter接入,有adapter接入时,后面DC/DC只工作在降压模式,因为要给电池充电,但是adapter拿走之后,要打开boost电路,必须要程序满足条件。
问题3:D+/D-是用来检测24195的输入接的是适配器还是电脑的USB口,如果是适配器,那么输入限流可以设置大一些,如果接的是USB2.0的口,那么输入限流在500mA。这是为了防止BQ24195把前面的供电设备拉垮。REG08-0A的数据,你可以用单片机通过I2C协议来直接读取。也可以使用官网上的上位机软件去读,不过使用上位机软件时,需要有一个GPIO转USB的adapter把你芯片和电脑连接起来。