This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:TPS54286芯片烧毁的可能原因

Expert 1795 points

Other Parts Discussed in Thread: TPS54286, DRV8412, DRV8812, TPS2420

TPS54286芯片,参照datasheet中,24V输入,5V、12V输出的电路图例子,略有改动,如果下面的描述不是芯片烧毁的原因,我再把电路图贴出来。

在PCB上,这块芯片的输入端和输出端都是通过插头连接的,所以有可能出现这么一种情况,就是芯片的输入端先接24V电源,然后5V、12V的负载才接入;也可能是一起同时接入的(就是插好接线后,打开总电源)。

在测试中发现,如果是插好接线后才开电源的,芯片都正常工作。但是如果接好24V输入,然后才接入负载的,在接入负载瞬间就很容易烧毁芯片,表现为24V的输入端引脚整个烧融了,芯片也是在这个引脚附近部分烧黑,已经烧两块。而且第二块烧毁时,连带负载的一块 C2000  MCU 也烧了,实在打击大了。

所以先请教一下,对于这类芯片,如果先接入输入电压,然后才突然接入负载,是否会有问题?实际上,由于是插头插入的,所以可能也不一定是插入顺序问题,还可能是插拔时有抖动,包括输入端和输出端都有抖动,这种抖动是否也会导致芯片烧毁?

负载端是数字逻辑器件、MCU、DAC芯片、LED指示灯之类,还有几块电机驱动芯片(DRV8412、DRV8812),都没有电感负载,不大可能开机瞬间有大电流,总负载也计算过,不会超过额定电流,正常工作时也没发生过 “过热保护” 的意外,而且TPS54286本身也各种自我保护,怎么会烧得那么惨烈?

  • 在24V存在,输出电压已建立的情况下, 拔插负载板属于热插拔情况, 若没有热插拔保护芯片如TPS2420的保护, 会在插拔瞬间产生大的dv/dt以及冲击电流(负载板电容瞬间短路状态). 输出电压可以震荡到两倍额定值. 冲击电压,电流足以打坏负载和电容等器件.

    因此,不建议热插拔负载板,除非有加热插拔保护线路.