LMR14206有时不启动发出嗞嗞响声,怎么回事 ?输入30V 输出3.3V 电流100MA 左右,请求解答。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的是30V输入 3.3V输出,如果把输入电压降为5V可以启动。30V输入的情况是有时正常启动,有时发出嗞嗞的响声
您好,根据您后面的描述,我认为是电感发出的声音,谢谢。
可以参考这个文档,比较系统
- http://wenku.baidu.com/view/57485c68a98271fe910ef946
liang wang6 说:什么原因导致电感发出声音呢?谢谢