This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请帮忙推荐一颗IC,感谢

Other Parts Discussed in Thread: BQ24072, BQ24075-Q1, BQ24270

您好,目前计划做一款行车记录仪,在电源管理这部分想请推荐一颗IC,需求和环境如下:

1.行车记录仪使用锂电池,3.3V-4.2V,容量很小,只有300mA,所以对充电电流要求不是很高,500mA就足够了,另外车上充电器最大输出只有1.5A/5V,AC,如果充电电流过大,同时系统耗电过大,车充可能会被拉挂掉。

2.需要在插入充电器后由充电器供电,拔掉充电器由电池供电,行车记录仪耗电峰值(peak)大概在1.2A左右。

3.最好可以不用连接I2C接口,当然如果没有合适的,带I2C也可以。

非常感谢