This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS71710DCK EN使能脚拉低别的电源芯片



如上图所示:TPS71710DCK 与TPS62260DDCR 的EN脚连在一起,现在的问题是:

上电后1.8V和1.0V都没有输出,发现是因为En脚低电平shutdown了。将:TPS71710DCK 焊掉后,EN回复高电平,上面的1.0V和1.8v即可输出。

请问到底是什么原因导致:TPS71710DCK 的EN变低了呢?然后导致TPS62260DDCR也被拉低。是否是芯片质量问题?若不是什么原因呢?请帮忙分析,谢谢~

备注:该设计已经在前两批制版中验证过没有问题,但后来再制版焊接 发现所有板子都是因为TPS71710DCK导致电源有问题,焊掉就好了。如果是设计问题,为什么前两次没有问题呢?