电源芯片需求如下:输入3.6V-5.25V,输出5.0V,输出电流1.8A, 纹波30mV以下,效率90%以上,开关频率在1MHz以上。
考虑选用的buck-boost芯片TPSTPS63020,存在的问题是boost模式下纹波电流比较大40mV, 低电压输入下效率比较差85%(3.6V输入)。
如果选用 100%占空比BOOST+直通,如TPS61253A,PWM模式下最大占空比视乎只能到97%,PFM模式下开关频率降低到500kHz以下会对系统造成干扰。
麻烦推荐一个更好的方案。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
避免不要boost状态的,无论是升降压中的升压,还是采用2步转换,后者效率也很可能达不到90%,因为也会用到boost,同时还会有一步降压,并且电路过于麻烦。
所以仍然建议用升降压芯片来做,不嫌麻烦可以选择TPS5176之类的升降压,效率非常高,但是电路复杂。
或者选择带有pass-through功能的升压芯片例如TPS61022, 效率也非常高, 推荐使用,可以强制PWM模式,如果不强制在输出增加一级LC(磁珠滤波器),纹波会小很多,只是这款芯片电流有些大,也就是电流保护形同虚设。