大家下午好!
现在有个项目的电池组参数是:电池组容量86Ah,短路保护电流38A,最大充电电流25A,最大放电电流10A,要带电量计量。
问题1:用BQ20Z95可以满足以上的参数设计吗?如果可以,容量、电流等的参数怎样设置?
问题2:如果BQ20Z95不能满足以上参数设计,大家有什么好的方案提供。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢Michael回复!
我用BQ34Z100已经用在其他项目做了样品送出,BQ34Z100在放电到了32%后SOC就会停止在此,不下降到0%了(按论坛上Sheldon Cai的指导是放电的32%时暂停放电后再继续放,这方法是可以使SOC下降到0%的)。现在这个客户可能也知道有怎样的现象,已经叫我不要用BQ34Z100做样品给他了。不知道其他工程师用的BQ34Z100项目会不会有左右的现象?是否有好的方法解决这个问题的?