LM3489为hysteretic mode DC-DC,看起来输出ripple会大一点,请问后续加电感电容滤波网络可以有效减小ripple吗?或者由什么其他办法?
另外sink电流比较大,不希望由于滤波网络引起较大drop。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在电容后面再加电感电容滤波网络应该会减小ripple但是肯定会影响变换器的响应速度
1、反馈电阻中,上面的电阻并联一个Cac,达到效果把Vout脚的脉动耦合到FB端。(可以试试看)
2、通过R和C串联以后并联于L,在R和C中间接一C到FB端。(no ripple required at output) (对变换器动态响应不利)
谢谢。
感谢提供的方案,该应用对响应速度要求不高,但是要求output ripple比较小。。。
请问第二种方案有实际试验过吗?
另外hysteretic mode 的DC-DC是不是比较挑Vout端电容?使用过程中有什么比较重要的注意的事项?
主要是想用这款设计Vout 5~20V可调电源,要求能够工作稳定,ripple较小就可以了...响应速度慢点可以接受...
您好,这个方案我倒是没有具体试验过,这是D-CAP模式减小输出脉动的方案,因为hysteretic 与 D-CAP 类似,所以你可以试试看。
另外你说的比较挑输出端电容是什么意思?
D-CAP2 是哪种模式呢?是否有相关技术文档...之前知道voltage mode,current mode,constant on time等。。。
另外由于设计需要满足 Vin:4.5~25V,Vout:4.5~20V,Iout 4A,maximum duty circle 100%,才选用这款DC-DC controller的...
似乎hysteretic mode DC-DC是靠Vout端 ripple来维持稳定switching,从datasheet上来看如果ESR太小会工作异常...
D-CAP mode 的芯片如TPS53355
D-CAP2就是讲我前面所述的纹波注入电路集成进D-CAP芯片得到的,芯片如TPS54327/8
我找了下D-CAP2 模式的DC-DC 似乎满足不了我上面提到的设计需求,找不到相应的规格...
看起来只能外部加您之前提到的那种纹波注入电路了,那这种纹波注入电路的R,C值该如何选取呢?是否有相应的计算公式...
如果额外加这部分电路,是否有导致DC-DC工作不稳定的风险...
D-CAP is the meaning of direct capacitive control technology.
D-CAP used constant on-time and the ripple of capacitive ESR to modulate the off-time. This solution can avoid the loop compensation design.
加这部分电路是不会导致DC-DC工作不稳定的。详细情况请参考这篇文章:
D-CAP(TM) Mode With All-Ceramic Output Capacitor Application
The TI D-CAP™ Mode controller is widely used in computing power management. D-CAP™ Mode requires an appropriate amount of equivalent series resistance (ESR) on output capacitors to ensure the loop stability. However, many customers prefer to use a low-ESR capacitor such as a ceramic output capacitor. Sufficient output ripple, however, may not be available in this case to ensure the system stability. This application report introduces an implementation of D-CAP™ Mode with all-ceramic capacitor application using a ripple injection approach. First, the basic D-CAP™ Mode operation is described. Then, the ripple injection approach is introduced to ensure system stability. Last, the step-by-step components selection procedure is provided. The performance of TPS53219EVM with all-ceramic output capacitor using ripple injection approach is demonstrated. This ripple injection approach can be applied to TPS51116, TPS51117, TPS51315, TPS51218, TPS53219, and other single D-CAP™ Mode controllers with low- output voltage application.
好的 原理图先按照这样设计 后续等PCB回来再调试
另外如果不加这部分纹波注入电路,而是按照datasheet中typical电路设计,vout电容ESR过小会导致什么情况?
首先开关频率会变小,影响你的电感设计,其次,ESR小电压纹波主要靠电容产生,与电感电流有相位差,输出电压到门限,开通关断开关管并不能马上让输出电压上升或下降。具体见LM3489datasheet
了解。。。另外我查了下您提供的这中纹波注入电路在constant-on time DC-DC (e.g. LM25085)datasheet typical电路中都有提到,可是似乎在 hysteretic mode DC-DC datasheet中没有看到该种应用...
您那边是否有过hysteretic mode 下应用该纹波注入电路实际经验?好像LM3489 Evaluation borad也没有预留这样的电路。。。
您好,手边暂时没有EVM板哎,
这边PCB最近就要送洗,也来不及在买EVM板回来实验了...
打算改用LM25085 Constant-ON time dc-dc,其datasheet typical电路中有使用到该纹波注入电路。。。这样应该会保险一点吧?
您好,
1、比较危险,裕量比较小。
2、电压尖峰跟您布线的密切相关,布线合理不合理电压尖峰相差很大。
3、可以考虑RC吸收电路减小电压尖峰。(并不能消除电压尖峰)
谢谢。欢迎补充指正。
增加电感电容滤波网络的确会改善滤波效果,但同时要注意,电感电容的加入可能会给电路带来其他的问题。设计时要选择合适的参数。
加电感电容滤波肯定能减小纹波,这个和电容的材质也有关系的!