Other Parts Discussed in Thread: TPS54560
公司最近设计了一款电路板,使用了TPS54560芯片,原理图是完全按照参考电路设计的,输入电压为27V,输出为3.3V,负载电流为1A,在常温下电路工作正常,当在-40度做低温工作实验时,所有的电路板输出的3.3V不正常,为2.2V左右。现在可以确认的是芯片焊接没有问题,负载在-40度是可以工作正常的,所以负载本身是没有问题的。我们一共焊接了10块电路板都是一样的现象。然后再高温55度工作时(中间通过烘干等正常的温度试验流程),有3块电路板的负载(芯片模块)直接短路,损坏了,不知道是什么原因造成的。在按照参考电路设计的过程中,将EN管脚悬空,因为我们输入的电压固定为27V,所以这样设计是没有问题的,最近我们将其中的一块电路板的EN管脚按照参考电路接到两个分压电阻之间,在低温-40工作时,电路板能正常工作,输出电压也为3.3V;其他电路板还没来得及处理。想问问大家,这种情况是哪里出问题了,我们的电路完全和参考电路一样(相关的参数已经通过计算确定);希望得到大家的帮助。