Part Number: UCC28780
Other Parts Discussed in Thread: UCC24612
我们使用UCC28780+Navitas GaN NV6115/NV6117+UCC24612设计,固定30V输出,最大输出功率70W。产品在生产后用输入240V,输出满载30V/2.34A的条件去做老化没有发现问题;但是如果在输出完全空载的条件下去做测试,产品会陆陆续续在1小时~3天内出现上MOS(NV6117)烧毁的现象,烧毁的MOS量测发现,多数有几欧到几百K的内阻,总不良率在5%左右。如果断电后重新再上电,仍然会有不良发生。
我们尝试在输出端加一个30mA的负载,同时在上MOS管NV6117的D、S之间并联一个47pF/1KV 0805的电容,用相同的条件测试7天,没有发现有上MOS烧毁的现象。
我们想了解,由于此设计已经通过了DOE VI的认证,在输出端加一个30mA的负载并不能满足认证的要求。是否TI有其它建议,可以改善这个问题?