This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: 在空载模式下会在1小时~3天内出现5%左右的上MOS烧毁

Part Number: UCC28780
Other Parts Discussed in Thread: UCC24612

我们使用UCC28780+Navitas GaN NV6115/NV6117+UCC24612设计,固定30V输出,最大输出功率70W。产品在生产后用输入240V,输出满载30V/2.34A的条件去做老化没有发现问题;但是如果在输出完全空载的条件下去做测试,产品会陆陆续续在1小时~3天内出现上MOS(NV6117)烧毁的现象,烧毁的MOS量测发现,多数有几欧到几百K的内阻,总不良率在5%左右。如果断电后重新再上电,仍然会有不良发生。

我们尝试在输出端加一个30mA的负载,同时在上MOS管NV6117的D、S之间并联一个47pF/1KV 0805的电容,用相同的条件测试7天,没有发现有上MOS烧毁的现象。

我们想了解,由于此设计已经通过了DOE VI的认证,在输出端加一个30mA的负载并不能满足认证的要求。是否TI有其它建议,可以改善这个问题?

  • HI

        将电路传上来看看?

  • 你有邮箱?我私发给你看看?

  • HI

        不能附件上来吗?  

  • HI

        有些不太清晰,有没有确认RCD电路,以及MOS的电压电流波形?

  • ACF的架构是将变压器的漏感能量回收,所以除了传统的下管外还增加了上管MOS,没有RCD。拍摄了小视频,分别有带载30mA、20mA与空载的上管DS波形,可以看出带载30mA时,上管的DS波形就很稳定了。这个与我们内部实验的结果一致,当带载30mA后去老化,没有发现不良;带载20mA或以下电流时上管有5%的几率会烧。

    链接:pan.baidu.com/.../1SnvHM0Nbtc4iOYDfxZLkfw
    提取码:trgk

  • HI

        我看的是参考电路,看错了,是没有RCD电路。

        上面的波形,是轻载下的吗?  有接近MOS  VDS耐压?

  • 输入电压为240Vac,示波器看到的上管Vds大约在570V左右,而纳微GaN NV6115的耐压是650V,还有一些余量。不过问题是不知道它什么时候会烧,也不是每一台都会烧,会烧的板大约在1小时~3天内有5%的几率会烧。看波形图,当带载30mA以上的电流后,上管Vds的波形很稳定;带载30mA以下,Vds的波形相当不稳定,频率不停在变化。我们怀疑是不是Ti的UCC28780 ACF控制器在空载条件下工作会不稳定,导致上管有烧掉的可能。工厂内用满载(2.34A)老化没有发现有上管烧掉的问题,只有在空载条件下静置会烧上MOS。烧上MOS的时候也有少部分的几率造成UCC28780烧毁。

  • Hi

        问题仅出在轻载,在美国E2E上问一下,应该是有设计问题的,我这边没有板子测试,很难看到问题。

        https://e2e.ti.com/