Other Parts Discussed in Thread: BQ76PL536
您好:
我的主芯片无法和BQ通过SPI通讯,HSEL接地,LDOD1 LDOD2 LDOA REG50都是5V。电路连接应该没有问题。主芯片可以通过SPI以广播的形式发送数据,但是BQ好像没有收到,两片BQ之间也没有检测到时钟信号。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如需TI官方的CRC校验函数及例程,请发邮件至:arvin.chang@bat-technology.com
我的SPI通讯是成功的,但是REG50引脚输出只有3V 不到5V 这是什么情况?
你好,我刚接触BQ76PL536,想请教两个问题。1、是否可以通过测量BQ芯片管脚电压判断芯片正常工作?2、如何判断MCU与BQ芯片通信成功。请给予解答。感谢
请问我在一个主机上只挂了一块BQ76pl536,我的CS_N接高,CS_S接低这样对吗,我只用一个这个BQ是不是就不用分配地址,而且我读到的值一直都是0xff