问题现象:
VCC,Vmppt,Vref,Vregn等电压都没有问题,但是红色LED一直闪烁,输出电压只有0.79V,另外HIDRV和LODRV上的NMOS在芯片上电后,G级和S级电压一样(导通?),电路板参照官方开发板设计,元器件基本上都是一样的。
---------------------------------------------------------------------------------------------------------
采购渠道:
分三个供应商(非官方指定供应商)12片,只有5片是正常的,其他都有此类问题(STAT1闪)?
---------------------------------------------------------------------------------------------------------
问题1:市面上的这块片子,非正规渠道采购的的假货比较多?
问题2:焊接有问题?但是好的片子从板上取下换在不好的板子上,还是好的,能正常工作(试过两片)。
问题3:坏的片子,SRN 窜入100欧姆电阻,有19.5mv压降(接上电池的情况下,万用表测),假如按照第18页流程,应该有0.8V 至0.2V之间压降才对?
问题4:电池欠压的情况下,30分钟预充电,充电电流是多大了?
问题5:有一次热插拔后,正常芯片板子也出现STAT1闪烁不能充电的情况;假如确认是芯片损坏,这种现象主要是什么地方出现问题,怎么通过外围保护解决?